Tool/software:
Hi Sanjay , did you ever mange to try this on the an EVM ?
I made another PCB design using the same part and I don't get any FSYNC clock at all.
I am using 24.576mhz oscillator MCLK on GPIO1 in master mode.
I am using internal LDO 1.8V and running IOVDD and AVDD on 3.3V
I would much appreciate it if you could try the EVM for this part and confirm that it is possible to use it in Bus Master mode with PLL active.
and if you get it to work , you could upload register settings and PP3 software file so I can try the settings on my hardware.
If I can't get the part to generate BCLK and FSYNC properly I will need to look at another vendor for a high dynamic range ADC
which would be a shame as I have to designs with this stumbling block.