Tool/software:
I found that both Address 0x02 and 0x4D are named VREF_CFG.
Do both locations need to have the same value written, or is the name of one of the addresses incorrect?
I found that the description of the 0x50 register function for TAC-5412-Q1 differs between the development software PurePath Console and the datasheet.
The datasheet indicates that bits 2-5 of register 0x50 are reserved,
while the development software shows that bits 2-5 have functions.