Part Number: TLV320DAC32
Other Parts Discussed in Thread: TLV320DAC3100
Tool/software:
Hi,
We are using a PDM microphone to capture audio, which is then processed in an STM32 microcontroller and sent to a DAC (TLV320DAC32). The DAC is connected to a 3.5mm audio jack to allow sound playback via headphones. Additionally, we have a volume control button connected to the STM32, which controls the volume of the DAC.
To implement this concept, I have been searching for a code example or driver for the TLV320DAC32 that is compatible with STM32 (ARM Cortex-M) microcontrollers. So far, I have only found Linux drivers for the TLV320DAC3100, which are complex and difficult to understand.
Could you please provide a simplified driver or code example for the TLV320DAC32 that I can use to develop on microcontrollers?
Thank you for your assistance.
Best regards,
Rajkumar