Other Parts Discussed in Thread: LM324, TPA6404-Q1
Tool/software:
Tool/software:
Pandian,
What is the source driving the 100kohm resistors? If the source output impedance is low the 100k and the LM324 circuits can be eliminated, and the source can be directly connected to all 4 inputs through capacitors. See the application schematic in the datasheet for the proper connections on the input.
Regards,
Gregg Scott
Hai, Gregg Scott,
Thanks for your reply.
The headphones' output (L &R) is directly connected to the 100k resistor.?
LM324 is required or not?
Regards,
Pandian
Hi Pandian,
You cannot connect the Left channel and Right channel of a source together. They need to summed together and then connected to the inputs of the TPA6404-Q1.
I am assuming the headphone output has Left and Right output and a shared ground. Place a 100K resistor in series with each output. Connect the other end of the 100K resistors together. This connection would go the 0.47uF capacitors on the application schematic in the datasheet. All the 0.47uF capacitors would be connected together at the input side, not the IC side.
Regards,
Gregg Scott