Other Parts Discussed in Thread: TSC2117
Tool/software:
Hi
I want to use PurePath studio to configure MiniDSP.
But when I download and run my project, no sound output.
Meanwhile if I use TLV320AIC3111EVM Software to control the board, it can output sound.
Is there something wrong with my projec?
the log is as follows:
Generating code for base_main_Rate44 .. assembling .....Done.
Generating patches...Done.
Build succeeded.
Found board type: FWIDTLV320AIC3111EVM-K.
Board sampling rate: 44100Hz.
Downloading base_main_Rate44.cfg to the EVM.
done.