Other Parts Discussed in Thread: TAS2505
Tool/software:
Hello, when I was using TAS2505, I noticed the 1.8V output port from the LDO produces about 2.7V if I connect the board via USB or provide a 5V voltage externally, and 2.7V is beyond the recommended maximum voltage (1.95V) specified on the datasheet for AVDD and DVDD. I was wondering if it is still ok to continue using 2.7V for AVDD and DVDD in this case, or if there's any workarounds.
Thank you!