Tool/software:
The MCLK(12.288MHz)/BCLK(1.536MHz)/WCLK(48KHz) is supplied from imx8mp(NXP) and data transmittedto codec, but there is no sound at playback.
The all clocks and data signal is OK.
We don't use external AVDD and DVDD (GND), but IOVDD 1.8V and LDOIN 3.3V only. Of course, LDO_SELECT pin is high(1.8V).
We refer to 4.0.2 In the TLV320AIC3254 Application Reference Guide((SLAA408A).
For our circuit using internal AVDD and DVDD rather than external, which register value have to changed?
Are there any other registers that have to be set other than the below?
- b[3]=0 in page 1 / register 1
- b[0]=1 in page 1 / register 2
- b[3]=1, b[0:1]=1 in page 1 / register 0x0a
- b[3]=1 in page 1 / register 0x33 for capture, not playback
Thanks.