Tool/software:
Hello, use tpa3116d2 to design the power amplifier, the load is 4ohm, the power supply is 24V, and the output L = 33uh, C = 0.68uf. PWM = 400khz.
SDZ and MUTE controlled via dsp.
Power-on sequence: 24V on--- > SDZ_HIGH --- > MUTE_LOW
When MUTE (LOW), the 3116 starts to work, observe the 24V power supply, and the current increases by 0.014A (no audio input, no load). Touch the 3116 chip Power∞ to warm up.
Is it normal?
I remember that this current is related to 33uh inductance, differential mode impedance, or common mode impedance.? But it can't be calculated, how to calculate it? Thanks...