Part Number: DRV595
Tool/software:
Hi all,
According to the absolute maximum rating of the data sheet, maximum Slew Rate of SDZ is 10V/ms.
In addition, the note (2) which seems to be due to current restrictions is written as follows;
100 KΩ Series Resistor is Needed if Maximum Slew Rate is Exceded.
What is the reason why MAXMUM SLEW RATE is restricted?
Is it necessary to protect this through rate when controlling SDZ directly with a CPU?
In this case, is it necessary to have a 100k ohm in series resistance?
When the power is launched, the SDZ is fixed to LOW.
Regards,
Toshi