Other Parts Discussed in Thread: TAS5825M
Tool/software:
Hi Arthur,
I'm using TAS2781_v3.0.1-beta.20 to configure my dual TAS2781 design. My goal is to generate a .cfg file which I can use to parse and load into the chips from the system microprocessor. Some questions:
- It appears that the Smart Amp section is not able to do anything without characterization data from the characterization board, even though I've entered all the speaker parameters by hand. Please confirm if this is expected behavior.
- Unlike the TAS5825M which I am using on my other project, there appears no way to import a measurement curve and automatically tune the biquads to it. Please confirm.
- When I examine all the .cfg files that it spits out, I'm confused as to which is the one that contains all the settings I would need to configure it from scratch. I think it is combined_configuration...TuningMode.cfg. Is this correct.
- Is there some already existing Linux or C code parser that can be used to convert the .cfg file to an I2c stream?
Thanks for your help,
James