This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

fail when TAS3308 SLAVE DOWNLOAD VIA I2C1 WITHOUT EPROM



 while SLAVE DOWNLOAD VIA I2C1 WITHOUT EPROM

 error info:

Generating code for main_Rate48 ..  assembling ... i2c table ... dsp init ..Done.
 building config file ... done.
Summary: 0 Errors
Build succeeded.
Downloading Slave config to the EVM ..Failed.
Slave load data failed at Line 2097, Memory type 0

why?

ProcessFlow1.cfg download fail,but slave_main_Rate48.cfg download successfully VIA I2C memory tool

1106.ProcessFlow1.cfg.rar

4336.slave_main_Rate48.cfg.rar