This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Speaker Amplifiers

[FAQ] TAS2563: Adjusting Digital Volume Control using I2C

[FAQ] TAS2563, TAS2562, TAS2557, TAS2770 Android/Linux Drivers Link

[FAQ] TAS2563: PDM Interface

[FAQ] TAS2563: What are the .ftcfg, .cfg, .h, .json, and .bin files used for in End System Integration?

[FAQ] TAS2505: Protection Flags and Interrupts

[FAQ] TAS2505-Q1: How to configure TAS2505/TAS2505-Q1 EQ biquads

[FAQ] TAS2563: How to use external boost PVDD voltage

[FAQ] TAS2563: How can I verify the excursion and thermal protections are function properly?

[FAQ] TAS2563: How can I read the resistance of the speaker, Re, from the devices registers?

[FAQ] TAS2563: I2C & SPI Setup (Not via USB)

[FAQ] TAS2563: Speaker cannot heat up properly during thermal characterization

[FAQ] TAS2563: Gain Control of Smart Amps in PPC3

[FAQ] TAS2563: What Tuning Tools are Available for TAS2563 in PPC3

[FAQ] TAS2563: How do use external PVDD to power the amplifier

[FAQ] TAS2770: Can the device drive DC output?

[FAQ] TAS2563: Component Selection Start Guide

[FAQ] Does TI have crosses for Infineon/Merus recent EOL or discontinued multi-level amplifiers like MA2306, MA2304, MA12070, MA12040, and IR431x?

[FAQ] Does TI have crosses for Cirrus Logic recent EOL or discontinued devices like CS536x ADC, CS43x5 DAC, WM8985/CS4243x Codec, CS842x SRC, and CS35L0x amplifiers?

[FAQ] Smart Amp

[FAQ] TAS Devices Information

[FAQ] What are some new & exciting parts that TI offers?

[FAQ] Does Texas Instruments support SoundWire solution for PC/Notebook applications?

[FAQ] TAS2120: What are the proper considerations when driving a high-inductance actuator with TI Class-D amplifiers?

[FAQ] [参考译文] [FAQ] TAS2563:PDM 界面

[FAQ] [参考译文] [常见问题解答] TAS2563:I2C &SPI 设置(不通过 USB)