so i was thinking i could use an OPA2544 on a mini pcba "pin swapper" and appropriate connections for pins that differ from the TCA 2465 to get a 9 pin sip package (5 tca’s were used and whomever designed the circuity that used it simply MONKEYED it!!!!!!!!!!!! Used as fan motor drivers, and environmental control (flapper) contol. They fail like mad and the TCA’s are just not available anymore so I think I could use this chip as a replacement or does anyone have a better thought(s)
HELP -pleeeeeeze! 1000's of units each using 5 tca's (or) opa's