Hello!
Call me stupid but I'm not getting how the sub- and sub+ outputs of the TAS5706b are meant to be used. I get a nice bass sound if I take either single one of them and apply an LPF with a ~300Hz cut-off frequency. The only difference I can see between the two is a minor phase shift.
Once and for all, which alternative below is true about the sub- and sub+ signal pair of the TAS5706b?
a) I can use either of them (doesn't matter which) and LPF that
b) I must logically AND them together and then LPF that
c) They two are differential outputs to minimize distortion and I must use a differential amplifier on them and then LPF that.
d) I should do something else. If so please explain what to do and how to do it
Could someone please tell my which option is true so that I can sleep well at night :-)
Thank you very much!