Dear Ti developers,
I faced the I2C communication when I fly-wire I2C pins to the TAS5713EVM.
The default I2C device address for TAS5713EVM is set to 0x36, using the TAS5713 GDE tool to read out the device address, by read out from register address 0xF9.
When i send the wrong device address (for example, 0x32) to the TAS5713EVM, the signal shown on the oscilloscope telling me that i received a 'LOW' from the SDA line, which indicates received ACK from TAS5713.
I believe the I2C clock communication speed is not the cause of it, as it is below 100kHz.
Please advice.
Thanks
Regards,
Chan