Hi,
1. I am trying to set a 4th-order notch filter using Pure Path using the cascaded biquads block.
I was able to make this filter work for primary AIS interface of tlv320aic3254 chip. Attched below are Mag vs frequency responses of
recorded audio on primary interface.
Without Notch Filter :
With Notch Filter at 4.2Khz:
2. I have trouble getting this filter work for the Secondary AIS interface of tlv320aic3254.
I do get audio on this Interface, but the frequency response shows that the filtering action has not taken place !!!
i.e. I don't see a dip at 4.2Khz in the Mag vs Frequency response.
3. I have no clue as what is going wrong.
I have attached the Pure Path text scripts (which I have modified to suit my hardware) using for primary and secondary AIS interface.
;----------------------------------------------------------------------------------- ; Software Reset ;----------------------------------------------------------------------------------- reg[ 0][ 1] = 0x01 ; Initialize the device through software reset reg[254][ 0] = 0x0a ; Delay 10ms ;----------------------------------------------------------------------------------- ; Configure Power Supplies ;----------------------------------------------------------------------------------- %%if (%%prop(TargetBoard) == 2) ; AIC3254EVM-U specific configuration reg[ 1][ 2] = 0xa9 ; Power up AVDD LDO reg[ 1][ 1] = 0x08 ; Disable weak AVDD to DVDD connection reg[ 1][ 2] = 0xa1 ; Enable Master Analog Power Control, AVDD LDO Powered %%else ; AIC3254EVM-K specific configuration reg[ 1][ 2] = 0x09 ; Disable weak AVDD to DVDD connection reg[ 1][ 1] = 0x08 ; Enable Master Analog Power Control reg[ 1][ 2] = 0x01 ; Disable weak AVDD to DVDD connection %%endif reg[ 1][ 71] = 0x32 ; Set the input power-up time to 3.1ms reg[ 1][123] = 0x01 ; Set REF charging time to 40ms (automatic) ; reg[254][0] = 0x28 ; Delay 40ms for REF to Power Up ;----------------------------------------------------------------------------------- ; Load miniDSP Code ;----------------------------------------------------------------------------------- PROGRAM_ADC ; miniDSP_A coefficients and instructions PROGRAM_DAC ; miniDSP_D coefficients and instructions ;----------------------------------------------------------------------------------- ; Signal Processing Settings ;----------------------------------------------------------------------------------- %%if (%%prop(SynchMode) == 1) ; SynchMode is enabled reg[ 0][ 60] = 0x80 ; DAC prog Mode: miniDSP_A and miniDSP_D ARE powered up together, miniDSP_A used for signal processing %%else ; SynchMode is disabled reg[ 0][ 60] = 0x00 ; DAC prog Mode: miniDSP_A and miniDSP_D NOT powered up together, miniDSP_A used for signal processing %%endif reg[ 0][ 61] = 0x00 ; Use miniDSP_A for signal processing %%if ("%%prop(FrameworkType)" == "AIC3254App8x4x") reg[ 0][ 17] = 0x08 ; 8x Interpolation reg[ 0][ 23] = 0x04 ; 4x Decimation %%endif %%if ("%%prop(FrameworkType)" == "AIC3254App4x2x") reg[ 0][ 17] = 0x04 ; 4x Interpolation reg[ 0][ 23] = 0x02 ; 2x Decimation %%endif %%if ("%%prop(FrameworkType)" == "AIC3254App2x1x") reg[ 0][ 17] = 0x02 ; 2x Interpolation reg[ 0][ 23] = 0x01 ; 1x Decimation %%endif IDAC = %%prop(miniDSP_D_Cycles) IADC = %%prop(miniDSP_A_Cycles) %%if (%%prop(miniDSP_A_Adaptive) == 1) reg[ 8][ 1] = 0x04 ; adaptive mode for ADC %%endif %%if (%%prop(miniDSP_D_Adaptive) == 1) reg[ 44][ 1] = 0x04 ; adaptive mode for DAC %%endif ;----------------------------------------------------------------------------------- ; Clock and Interface Configuration ;----------------------------------------------------------------------------------- ; USB Audio supports 8kHz to 48kHz sample rates ; An external audio interface is required for 88.2kHz to 192kHz sample rates ;----------------------------------------------------------------------------------- %%if (%%prop(SampleRate) == 176400 || %%prop(SampleRate) == 192000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x00 ; DOSR = 32 (MSB) reg[ 0][ 14] = 0x20 ; DOSR = 32 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x88 ; MADC = 8, divider powered on reg[ 0][ 20] = 0x20 ; AOSR = 32 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 88200 || %%prop(SampleRate) == 96000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x0f ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x00 ; DOSR = 64 (MSB) reg[ 0][ 14] = 0x40 ; DOSR = 64 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x88 ; MADC = 8, divider powered on reg[ 0][ 20] = 0x40 ; AOSR = 64 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 44100 || %%prop(SampleRate) == 48000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x0f ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x00 ; DOSR = 128 (MSB) reg[ 0][ 14] = 0x80 ; DOSR = 128 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x88 ; MADC = 8, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 32000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x00 ; DOSR = 192 (MSB) reg[ 0][ 14] = 0xc0 ; DOSR = 192 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x8c ; MADC = 12, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 22050 || %%prop(SampleRate) == 24000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x01 ; DOSR = 256 (MSB) reg[ 0][ 14] = 0x00 ; DOSR = 256 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x90 ; MADC = 16, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 16000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=24 reg[ 0][ 6] = 0x18 ; P=1, R=1, J=24 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x01 ; DOSR = 384 (MSB) reg[ 0][ 14] = 0x80 ; DOSR = 384 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x98 ; MADC = 24, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 11025) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=16 reg[ 0][ 6] = 0x10 ; P=1, R=1, J=16 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x02 ; DOSR = 512 (MSB) reg[ 0][ 14] = 0x00 ; DOSR = 512 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0xa0 ; MADC = 32, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 8000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=24 reg[ 0][ 6] = 0x18 ; P=1, R=1, J=24 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x03 ; DOSR = 768 (MSB) reg[ 0][ 14] = 0x00 ; DOSR = 768 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0xb0 ; MADC = 48, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif ;----------------------------------------------------------------------------------- ; ADC Channel Configuration ;----------------------------------------------------------------------------------- ;reg[ 1][ 51] = 0x40 ; Mic Bias enabled, Source = Avdd, 1.25V %%if (%%prop(TargetBoard) == 2) ; AIC3254EVM-U specific configuration reg[ 1][ 52] = 0x10 ; Route IN2L to LEFT_P with 10K input impedance reg[ 1][ 54] = 0x40 ; Route CM1L to LEFT_M with 10K input impedance reg[ 1][ 55] = 0x10 ; Route IN2R to RIGHT_P with 10K input impedance %%else ; AIC3254EVM-K specific configuration reg[ 0][ 28] = 0x00 ; Disable weak AVDD to DVDD connection reg[ 0][ 29] = 0x14 ; Disable weak AVDD to DVDD connection reg[ 1][ 10] = 0x7b ; Disable weak AVDD to DVDD connection ;reg[ 1][ 2] = 0x09 ; Disable weak AVDD to DVDD connection reg[ 1][ 51] = 0x58 ; Disable weak AVDD to DVDD connection reg[ 1][ 52] = 0x04 ; Route IN1L to LEFT_P with 10K input impedance reg[ 1][ 54] = 0x04 ; Route CM1L to LEFT_M with 10K input impedance reg[ 1][ 55] = 0x10 ; Route IN1R to RIGHT_P with 10K input impedance reg[ 1][ 57] = 0x10 ; Disable weak AVDD to DVDD connection4 reg[ 1][ 59] = 0x35 ; Disable weak AVDD to DVDD connection reg[ 1][ 60] = 0x35 ; Disable weak AVDD to DVDD connection %%endif ;reg[ 1][ 57] = 0x40 ; Route CM1R to RIGHT_M with 10K input impedance ;reg[ 1][ 59] = 0x35 ; Enable MicPGA_L Gain Control, 0dB ;reg[ 1][ 60] = 0x00 ; Enable MicPGA_R Gain Control, 0dB reg[ 0][ 81] = 0xc0 ; Power up LADC/RADC reg[ 0][ 82] = 0x00 ; Unmute LADC/RADC ;----------------------------------------------------------------------------------- ; DAC Channel Configuration ;-----------------------------------------------------------------------------------
;----------------------------------------------------------------------------------- ; Software Reset ;----------------------------------------------------------------------------------- reg[ 0][ 1] = 0x01 ; Initialize the device through software reset reg[254][ 0] = 0x0a ; Delay 10ms ;----------------------------------------------------------------------------------- ; Configure Power Supplies ;----------------------------------------------------------------------------------- %%if (%%prop(TargetBoard) == 2) ; AIC3254EVM-U specific configuration reg[ 1][ 2] = 0xa9 ; Power up AVDD LDO reg[ 1][ 1] = 0x08 ; Disable weak AVDD to DVDD connection reg[ 1][ 2] = 0xa1 ; Enable Master Analog Power Control, AVDD LDO Powered %%else ; AIC3254EVM-K specific configuration reg[ 1][ 2] = 0x09 ; Disable weak AVDD to DVDD connection reg[ 1][ 1] = 0x08 ; Enable Master Analog Power Control reg[ 1][ 2] = 0x01 ; Disable weak AVDD to DVDD connection %%endif reg[ 1][ 71] = 0x32 ; Set the input power-up time to 3.1ms reg[ 1][123] = 0x01 ; Set REF charging time to 40ms (automatic) ; reg[254][0] = 0x28 ; Delay 40ms for REF to Power Up ;----------------------------------------------------------------------------------- ; Load miniDSP Code ;----------------------------------------------------------------------------------- PROGRAM_ADC ; miniDSP_A coefficients and instructions PROGRAM_DAC ; miniDSP_D coefficients and instructions ;----------------------------------------------------------------------------------- ; Signal Processing Settings ;----------------------------------------------------------------------------------- %%if (%%prop(SynchMode) == 1) ; SynchMode is enabled reg[ 0][ 60] = 0x80 ; DAC prog Mode: miniDSP_A and miniDSP_D ARE powered up together, miniDSP_A used for signal processing %%else ; SynchMode is disabled reg[ 0][ 60] = 0x00 ; DAC prog Mode: miniDSP_A and miniDSP_D NOT powered up together, miniDSP_A used for signal processing %%endif reg[ 0][ 61] = 0x00 ; Use miniDSP_A for signal processing %%if ("%%prop(FrameworkType)" == "AIC3254App8x4x") reg[ 0][ 17] = 0x08 ; 8x Interpolation reg[ 0][ 23] = 0x04 ; 4x Decimation %%endif %%if ("%%prop(FrameworkType)" == "AIC3254App4x2x") reg[ 0][ 17] = 0x04 ; 4x Interpolation reg[ 0][ 23] = 0x02 ; 2x Decimation %%endif %%if ("%%prop(FrameworkType)" == "AIC3254App2x1x") reg[ 0][ 17] = 0x02 ; 2x Interpolation reg[ 0][ 23] = 0x01 ; 1x Decimation %%endif IDAC = %%prop(miniDSP_D_Cycles) IADC = %%prop(miniDSP_A_Cycles) %%if (%%prop(miniDSP_A_Adaptive) == 1) reg[ 8][ 1] = 0x04 ; adaptive mode for ADC %%endif %%if (%%prop(miniDSP_D_Adaptive) == 1) reg[ 44][ 1] = 0x04 ; adaptive mode for DAC %%endif ;----------------------------------------------------------------------------------- ; Clock and Interface Configuration ;----------------------------------------------------------------------------------- ; USB Audio supports 8kHz to 48kHz sample rates ; An external audio interface is required for 88.2kHz to 192kHz sample rates ;----------------------------------------------------------------------------------- %%if (%%prop(SampleRate) == 176400 || %%prop(SampleRate) == 192000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x00 ; DOSR = 32 (MSB) reg[ 0][ 14] = 0x20 ; DOSR = 32 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x88 ; MADC = 8, divider powered on reg[ 0][ 20] = 0x20 ; AOSR = 32 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 88200 || %%prop(SampleRate) == 96000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x0f ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x00 ; DOSR = 64 (MSB) reg[ 0][ 14] = 0x40 ; DOSR = 64 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x88 ; MADC = 8, divider powered on reg[ 0][ 20] = 0x40 ; AOSR = 64 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 44100 || %%prop(SampleRate) == 48000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x0f ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x00 ; DOSR = 128 (MSB) reg[ 0][ 14] = 0x80 ; DOSR = 128 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x88 ; MADC = 8, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 32000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x00 ; DOSR = 192 (MSB) reg[ 0][ 14] = 0xc0 ; DOSR = 192 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x8c ; MADC = 12, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 22050 || %%prop(SampleRate) == 24000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=8 reg[ 0][ 6] = 0x08 ; P=1, R=1, J=8 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x01 ; DOSR = 256 (MSB) reg[ 0][ 14] = 0x00 ; DOSR = 256 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x90 ; MADC = 16, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 16000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=24 reg[ 0][ 6] = 0x18 ; P=1, R=1, J=24 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x01 ; DOSR = 384 (MSB) reg[ 0][ 14] = 0x80 ; DOSR = 384 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0x98 ; MADC = 24, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 11025) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=16 reg[ 0][ 6] = 0x10 ; P=1, R=1, J=16 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x02 ; DOSR = 512 (MSB) reg[ 0][ 14] = 0x00 ; DOSR = 512 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0xa0 ; MADC = 32, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif %%if (%%prop(SampleRate) == 8000) reg[ 0][ 5] = 0x91 ; P=1, R=1, J=24 reg[ 0][ 6] = 0x18 ; P=1, R=1, J=24 reg[ 0][ 7] = 0x00 ; D=0000 (MSB) reg[ 0][ 8] = 0x00 ; D=0000 (LSB) reg[ 0][ 4] = 0x03 ; PLL_clkin = MCLK, codec_clkin = PLL_CLK, PLL on reg[ 0][ 12] = 0x88 ; MDAC = 8, divider powered on reg[ 0][ 13] = 0x03 ; DOSR = 768 (MSB) reg[ 0][ 14] = 0x00 ; DOSR = 768 (LSB) reg[ 0][ 18] = 0x02 ; NADC = 2, divider powered off reg[ 0][ 19] = 0xb0 ; MADC = 48, divider powered on reg[ 0][ 20] = 0x80 ; AOSR = 128 reg[ 0][ 11] = 0x82 ; NDAC = 2, divider powered on %%endif ;----------------------------------------------------------------------------------- ; ADC Channel Configuration ;----------------------------------------------------------------------------------- ;reg[ 1][ 51] = 0x40 ; Mic Bias enabled, Source = Avdd, 1.25V %%if (%%prop(TargetBoard) == 2) ; AIC3254EVM-U specific configuration reg[ 1][ 52] = 0x10 ; Route IN2L to LEFT_P with 10K input impedance reg[ 1][ 54] = 0x40 ; Route CM1L to LEFT_M with 10K input impedance reg[ 1][ 55] = 0x10 ; Route IN2R to RIGHT_P with 10K input impedance %%else ; AIC3254EVM-K specific configuration reg[ 0][ 52] = 0x04 ; Seconday Wclk = MFP5 reg[ 0][ 55] = 0x10 ; Secondary Output = MFP4 reg[ 0][ 31] = 0x20 ; Secondary MUX for Wclk = GPIO/MFP5 & Secondary MUX for Bclk = SCLK/MFP3 reg[ 0][ 32] = 0x0e ; AIS will use secondary interface settings reg[ 0][ 33] = 0x3d ; Secondary Data output from Serial Interface reg[ 0][ 29] = 0x04 ; Force AIS output the respective secondary clks reg[ 0][ 27] = 0x20 ; 24-Bit format on I2S reg[ 1][ 10] = 0x7b ; 0.75 V common mode ;reg[ 0][ 61] = 0x01 ; Processing block 1 for ADC, IIR with flat response ;reg[ 1][ 61] = 0x64 ; ADC PowerTuneMode 3 reg[ 1][ 51] = 0x58 ; Mic Bias 1.45 V reg[ 1][ 52] = 0x10 ; Route IN1L to LEFT_P with 10K input impedance reg[ 1][ 54] = 0x10 ; Route CM1L to LEFT_M with 10K input impedance reg[ 1][ 55] = 0x04 ; Route IN1R to RIGHT_P with 10K input impedance reg[ 1][ 57] = 0x04 ; Disable weak AVDD to DVDD connection4 reg[ 1][ 59] = 0x2a ; Disable weak AVDD to DVDD connection reg[ 1][ 60] = 0x2a ; Disable weak AVDD to DVDD connection %%endif ;reg[ 1][ 57] = 0x40 ; Route CM1R to RIGHT_M with 10K input impedance ;reg[ 1][ 59] = 0x35 ; Enable MicPGA_L Gain Control, 0dB ;reg[ 1][ 60] = 0x00 ; Enable MicPGA_R Gain Control, 0dB reg[ 0][ 81] = 0xc0 ; Power up LADC/RADC reg[ 0][ 82] = 0x00 ; Unmute LADC/RADC ;----------------------------------------------------------------------------------- ; DAC Channel Configuration ;-----------------------------------------------------------------------------------
Can someone please help in reviewing this script, particularly for the secondary interface.
I am not sure above scripts are sufficient to debug the problem, please do inform if any further details are needed.
Thanks,
Brontok :)