Hi teams:
I am puzzled about DIR9001. If I make the DIR9001 work in XTI mode, how can I use just MCLK. I connect the DIR9001's I2S to AIC3254. If I make the AIC3254 work in master mode. There will be two clock in LRCLK and BCLK pin.
If I use 24.566MHz Oscillation, the DIR9001 output sample frequency is 96KHz.. I connect the DIR9001's I2S to Tas5713 , but the Tas5713 the Supports 8-kHz to 48-kHz Sample Rate. Because I want to use CALCULATION OF ACTUAL SAMPLING FREQUENCY, I must use 24.566MHz Oscillation from the datasheet. So what can I do?