The 8520 configuring software with the tas5717 selected generates this line of code
w 36 1B 00 # set factory trim.
this is not consistent with the address of the tas5717 which is 54 or 56 depending on the state of the address line which we have tied low meaning it should be 54. When the program initially installed the 5717 config file was absent from the audio devices subdirectory. Any thoughts on what is going on in the configurator?