I have a TAS5707EVM on hand, however after we setup the whold test system, we may use the PC TAS570X GDE to initial the evaluation board, but we cann't hear any sound or music from the TAS5707A. I have tested the following step, I use the analog source, I aslo jumped JP4 AND JP5 TO adc, I used the LIN AND RIN as a audio input.
1, I tested the I2C communication, it looks ok, we may read the first address 0x00 value is 6c
2, I also tested the SCLK AND LRCLK , both with clock signal
3, No audio from the TAS5707A, I need your help to sovle the problem on the EVM.
Would you tell me where's problem or what i can do the measure it agian.