Dear Sir,
Is there EQ GUI tool can help TAS5508C EQ fine tune ?
ALE 5.2 generated EQ file format is not same as TAS5508C EVM tool.
Many thanks !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Terry,
For mature devices, we are not developing new tools.
The tools are much better for the newer devices, TAS5548 and TAS5558. I suggest you look into those devices.
-d2
Hello Terry:
I'm not sure what you mean by the format is not the same.
ALE 5.2 gives you 20 biquad coefficients but it arranges the biquads in 5 rows with 4 bytes of coefficients per row.
The TAS5508C GUI has only one row with a register number preceeded by "X" and followed by 20 bytes.
If you want to use ALE 5.2 and convert to TAS5508C format, this is the following format:
XYY ZZ ZZ ... ZZ
X - is required to denote a new register
YY - register number
ZZ - byte of data (for the EQ biquad, there are 20 bytes; ALE 5.2 first 4 bytes on the top line go to the first 4 bytes right after the register number in the GUI format, and so on).
Best regards,
Tuan
Hi, Terry,
This might help you:
Use ALE5.2 and save it as cfg file in the below format and use the tool to download to the device.
XYY ZZ ZZ … ZZ
X – must have this character capitalized
YY – the register number
ZZ – the 20 bytes data for the coefficients
-d2
Hi Don Dapkus,
Would you suggest how to set DRC for TAS5508 GUI ?
I use ALE to generate a DRC file for TAS5508 GUI and load it, can't see any effect ?
Many thanks a lot !