Other Parts Discussed in Thread: PCM3168A, PCM3168
hai
am venkat , we are planning to work with pcm3168a audio codec
i have doubt regarding the set up of pcm3168a .
1) if i set pcm3168 as master ,how it will generate the 'BCK'
2)how to set the sampling frequency to '96 khz'
3) if i give external 'SCK' , then bck will generate automatically r we need to set any register
4)whether we can use pcm3168a audio codec with blackfin BF548
5)is there any evaluation kit available?
specifications:
24 bit,
sampling rate - 96KHZ
Bck - 128*fs
128 *96
12.288 MHz
please replay back as soon as possible.'sachin@eilabs.co.in'
Thanks and Regards
venkatesh