Hi members.
This is BEN.
My customers is using TAS5717 for monitor.
It is a question to success with further TAS5717 for the next model.
《Q》
TAS5717 is include a DSP.
How quantization accuracy are either constituted by the DSP ?
◆For example
I suppose the datasheet p31【26-bit 3.23 Number Format】.
・sign 1bit , integral 2bit , point-unit 23bit
Is there any room in the head ? 2bit(12dB)?
Best regards
BEN.