Hello,
I am designing an amplifier around the TAS5613 IC in BTL using BD modulation, and have a question about selection of the output inductor. The inductor specified in the reference design is a Toko C3B-A0336, 10uH, 30mOhm DCR and 5A max. This part is not available through my preferred supplier (Digikey), and was hoping this part would be an acceptable replacement: Talema SW260C-5.0-10, 10uH, 25mOhm DCR and 5A max. They're designed for NI's simple switcher 260kHz systems.
http://www.toko.co.jp/products/pdf/inductors/c3b_amp.pdf
http://www.alfamag.com/PDF/InductorsChokes/Power%20Inductors%20&%20Chokes/SW260_Series.pdf
Without having the core material specified, does this look like it should be an acceptable replacement?
Thanks,
Dave Williams