This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

(Split) PCM5141 96K not working

Other Parts Discussed in Thread: PCM5142, PCM5141

Hi Matt,
I see the original thread has been closed related to PCM5142/5141. I would like to continue with some more questions in relation to this....
We are having problems with the PCM5141 and 96khz config (havent attempted 192k yet).
What works: Dumping the pps reg values generated from GDE for 48kHz. The PCM5141 outputs audio at 44.1 and 48k no problem as expected.
What doesn't work: Dumping the pps reg values generated from GDE for 96kHz. These is no audio output when using 96k I2S input.

Perhaps you have some pointers? I know there are some limitations to the default configuration, however we are using our own stripped back generation of the pps (5band eq and volume only).
We are starting to test this on the eval board now also.
Cheers,