This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5614A power into 8Ω at 1% THD

Other Parts Discussed in Thread: TAS5614A

Hi,

The description for the TAS5614A says it delivers 65W Stereo into 8Ω at 1%THD+N (5th bullet on this page).

However, when you look at the charts on the datasheet (Figure 1 on page 11), it looks much more like 75W.

Which is the correct spec?

Thanks,

- m

  • Hi Matt,


    The bullets on the front page of the d/s say 65W into 8-ohms at 1%. The plots make it look like it's closer to 70W. Depending on the system design, you might make 70W at 1%.

    Regards,

      -Diego Meléndez López
       Audio Applications Engineer