Hello to everybody !
I bought a TAS3308EVM-LC two weeks ago and I'm now trying to evaluate some simple tone generators.
I have this problem:
I use the GDE "generic-init" block to set several 3308 internal registers,
but the board seems to ignore the resulting "dsp_init_cmds.object" file.
For sure this file is properly prepared by the GDE builder (I see the right stuff opening it with a text editor)
but for some reason it is not able to initialize the 3308, even if it appears correctly embedded into the .image hex file.
I can initialize the chip only by sending the same registers values using the GDE "I2C Command Tool".
According to the init.c code, in the "generic-init" properties I set always "handler = 1" to invoke the I2C_write_32bit function,
"priority = 4" for the last instance I would like to send to the 3308 and "priority = 1" for all the other instances.
Is there anybody that face the same problem or has a solution ?
I'm using GDE 1.82 build 5.
Thank you.
Kind regards,
Marco Rampin