Hello, TI!
I was looking TAS3308 datasheet, and found on page 4 (application information) two "VR_ANA2" pins and two "AVSS_PLL"pins. Is it right ?
With best regards, Vladimir.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Vladimir Timohin said:Is it right ?
Vladimir,
You are correct. There are two pins that are pined out to allow for the user to add of external capacitors for bulk supply / decoupling. VR_ANA [pin #88], and VR_ANA2 [pin #83]. I have attached the schematic of our evaluation module for your reference.
Hi,
I'm trying to interface temperature and humidity sensor to cc2530 , This sensor needs bi directional pin and clock pin.
so I planned to use P1_0 as data and P1_1 as clock..
This sensor needs 8MHz on the clock pin so how to genarate this frequency on this channel..?
pls help