This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is a bug in a documentation for PCM3168 and in User's Guide for motherboard for PCM3168 . How this circuit converts differential signal to single-ended? You should add some DC on non-inverted input, if not signal after conversion has reference voltage on AGND and negative part of the signal is cutting off.
This is a part of User's Guide for motherboard for PCM3168:
This is a part of PCM3168 datasheet:
Could you explain this strange situation?
Hi Justin,
"The PCM3168 board has a +/-15 V supply for the opamps, so the output can be centered around AGND, without clipping" this is simply not true. See this part of circuit:
Where you see +/-15 V supply?pcm3168a_motherboard.pdf
How? This motherboard has fixed connection op amp supply to asymmetrical voltage. This is simply huge bug on PCB and it comes straight from datasheet. Few years ago I had sad surprise with DRV8432 - in datasheet first pin is show in two different places, moreover ESD protection of DRV8432 is terrible.Justin Bohr said:If you want to use the single ended output, you will need to add a negative supply for the opamp.
Thanks for your answers Justin
Pawel
Justin,
It is not solution for my problem. I have my own PCB with positive supply 5 V and negative GND (single supply), I connected VCOMAD pin as above. Does it is good approach? Output is connected to TDA8551 and everything seems to be good. TDA8551 has Vref = Vp/2 = 2,5 V and VCOMAD = 2,5 V so signal on the output is such as I expected.
Justin you are generating so many answers but you not help me at all. Can you finally refer to my solution?
Paweł