Hi,
I have a 3308 EVM LC connected to a board with 4 class d amplifiers and input section.
I am feeding an optical signal into my board and this is decoded via a DIR9001 IC as on the MC57xxPSIA.
My board works fine when i go from optical throught the 9001 into the class d power amps (2 off each, TAS5706 and TAS5602).
It also works when i go analogue in to the 3308EVM and take the I2S out to my digital amps also works.
however i want to have the 3308 process my optical input signal.
When i connect the I2S out from the 9001 and go into the I2S on the 3308. i get no digital signal on the outputs. I have all 3 clocks on the outputs that are correct in frequency.
Im sending in a digital signal on all 3 inputs.
I have set the 3308 to slave mode and forced it to only accept 48kHz which is what i am feeding to it.
Also i have tryed taking the digital in signal and outputting to headphones in the GDE but still no audio.
Everything looks fine and im sure i have set the 3308 up correctly.
Does anyone have any idea why i am getting no digital audio to pass through the EVM?