Other Parts Discussed in Thread: TAS5704, TAS5601, TAS5711, TAS5731, TAS5760M, TAS5754M
Application : electonic black board
Title : Product within specification recommended cases.
There are two of the specifications under consideration, and will have the ability to choose one.
1) High Output 2.1 ch : L/R: 20~25W/ch , SubWoofer: 20~30W , THD Under 0.5%
2) Low Output 2.1 ch : L/R: 10~15W/ch , SubWoofer: 15~30W , THD Under 0.5%
Device Question
1) High Output 2.1 ch : L/R: 20~25W/ch , SubWoofer: 20~30W , THD Under 0.5%
-> TAS5704 + TAS5601 or TAS5704
=> TAS5704 is configured BTL MODE and SE 2.1 MODE. Which would like to know for two modes. (2.1ch, L/R: 20~25W/ch , SubWoofer: 20~30W mode) If this is not with output specs(SE2.1), the following specifications to ensure that they can be applied.
2) Low Output 2.1 ch : L/R: 10~15W/ch , SubWoofer: 15~30W , THD Under 0.5%
-> TAS5704 or TAS5711 or TAS5731
=> Left picture is TAS5711, Right Picture is TAS5731,,, Both of them,,, 2.1CH spec..
Two please recommend device of the corresponding device (2.1CH / L/R : 20~25W/ch, Subwoofer : 20~30W)