This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to use the PCM3168a in slave mode to convert some MEMS microphone signals to I2S streams. I have connected the USBStreamer by the company miniDSP to SCKL,BCKAD,LRCKAD and DOUT1. The MEMS microphone is attached to VIN1+ and VIN1- via the interface circuit from Figure 58. I have buffered the supply ports as recommended in Figure 54. Mode is connected to ground. Unused analog inputs are connected to ground. DIN1…DIN4, RST, OVF, Zero, MC, MS, LRCKDA, BCKDA, MDI, MDO, VOUT1…VOUT8, DOUT2, DOUT3 are not connected.
VCC to GND is 5V, VDD is supplied by a 3.3V voltage regulator.
I don't get any signal out of the PCM3168a. It does never get warm when I apply the supply voltage. What am I doing wrong?
Thanks a lot!
Jack
I tried to debug the issue by measuring the pin voltages. Is it possible that I need to keep RST high the whole time in order to keep the codec running? I would really appreciate an example of a minimal application around the PCM3168a. I thought that I do not need any control pins if I operate the device under default the settings.
Thank you!
Jack
Ok, I am holding RST at VDD=3.3V now and I finally get some output. The problem now is that it is the wrong output. the microphone signal is totally lost, I only get some impulse every 10ms. I attached a picture of the signal plot.
I thought maybe this is some clock related issue? The device is running in slave mode. I don't write to the register settings, so everything should be running in default settings. Sampling frequency Fs is 96kHz, BCKAD is 64xFs, System Clock is 256xFs.
Hi Justin,
Thank you for the reply. I have attached a screenshot from my eagle schematic file. To the left I have connected the microphones via the amplifier circuits as mentioned earlier in this thread. I don't drive any I2C lines at all. Do I need to transmit any I2C signals if I just want to use the codec in default modes?
Thank you!
Jack
I managed to get some sound recorded using the codec now. I have attached two 96 kHz wav files, one the original recording from the codec, the other one a clipped version. Due to the advice from Luis Fernando I am now certain that that nuisance noise comes from DGND and AGND being connected to the same ground plane. It would be nice if you could listen to the recordings and see whether you can argue against my suspicions.
Thank you!
Jack