Good morning,
given that I am new to this world, I'll tell you my problem.
I have an EVM TAS5508-5142K7 and I have to connect it to a BT audio module Bluecreation BC127 on digital output (PCM / I2S/SPDIF).
BC127 TAS5508 BOARD (CONN. J60)
PCM_SYNC (46) => WS => (13) LRCLK
PCM_CLK (47) => BCLK => (11) SCLK
PCM_OUT (48) => Data => (4) SDIN1
GND (1) => (1) GND
SPI_PCM # (45) is grounded
BC127 I2S is selected and configured in Master mode, Left Justified with 1 Bit delay, 16 bps with a Word clock (WCLK) at 44100Hz and a Bit clock (BCLK) at 2.822Mhz (64*44100Hz)
After having properly set the BT module for digital audio output (i2s) I still can not make play audio.
TAS5508 BOARD is connected to the INPUT-USB board with the J40 connector and to the PC with the USB cable.
The only connection I can not do is to (2) MCLK because the BC127 module does not support it, but the MCLK is optional for i2s ..
I mistake or forget something?
Grazie in anticipo e a disposizione per fornire maggiori dettagli