This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320DAC3120EVM configuration

Other Parts Discussed in Thread: TLV320DAC3120EVM-U

We are using this DAC part in our project.

Our Processor is connected to the DAC using I2C & I2S interfaces and we want to drive output via the 8 ohm Speaker Only .

We have loaded the registers from the Init-script which is given in TI EVM TLV320DAC3120EVM-U . We have disabled the HP registers and increased the DAC volume control register.

All the clocks Mclk (11.2896MHz), Bclk(2.8224MHz),  Wclk(44.1KHz) and also DIN are given properly from the Processor to the DAC but not able to receive any  output.

 

Please share if possible  the Correct Registers configurations needed  to drive the Speaker.