We have 3 analog audio technologies that we want them to be made into 3 ICs. which TI department or appropriate person should I contact?
1. We can convert 5.1 surround sound into left and right channels so listener can hear surround sound with a pair of REGULAR headphones or stereo speakers. No upgrade or additional equipment is required.
2. Our amplifier is driven by both current and voltage. This amplifier can remove 80% (100% in a few months) of the back EMF error produced by the speakers.
3. Our Sonic Image Sound projector can produce surround sound effect with 2 full range speakers within a single enclosure. It is not a sound bar or using reflection of the walls.
Details can be found on our web site www.psychoacousticsolution.com. Pass word of the demo page is "test1" without the " ". If you have question, please email me at wwong@psychoacousticsolution.com.