Hi TI experts,
Currently I am tuning the TAS5782MEVM, but there are few functions that I don't really understand the details and relationship between them. Could you help to explain them ?
1) DPEQ :
a) Why there are 2 different Threshold ( Low & High ) ? what are these for and how to apply it ?
b) Why there are two EQ ( Low Level & High Level ) ? what are these for and how to apply it ?
c) Is this DPEQ will affect the setting of the "Equaliser" section ?
2) DRC : Why there are 2 Threshold regions ( 1 & 2 ) ? what are these for and how to apply it ?
3) AGL : AGL provide further protection for the amp after DRC ?
4) Clipper :
a) Is this function for clipping prevention ?
b) According to the document "TAS5782M Process Flow", it shows there are 2 input setting ( THD Clipper & Fine Volume ) , but there is only one setting ( Clipper Level ) in Clipper window in the actual PPC3-TAS5782EVM software. So I just need to adjust (Clipper Level ) only that PPC3-TAS5782MECM software provide in the window ?
5) DRC , AGL , Clipper : Are these functions are similar and aim to provide further protection for the amp step by step according to the block diagram flow ?
Thank you
Fai Chan