This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS3308 and EEPROM page size

Other Parts Discussed in Thread: TAS3308

Hello,TI!

I bought  TAS3308 EVM. There was EEPROM 24LC512xxx by MICROCHIP.

I try to change EEPROM to  AT24C64(my project is very small).

When i download code i see follow message:

-----------------------------------------------------------

Downloading image to the EVM ...
Verify failed.

 Bad: 0 61 122 183 244 305 366 ...........................

-----------------------------------------------------------

I know, that  EEPROM  AT24C64 have another PAGE SIZE (32 bytes instead 128 bytes in 24LC512xxx).

Is it possible to build image for EEPROM with 32 bytes  page size?

Or i have to use EEPROM with 128 bytes page size ONLY?

Thank you!