Hi,
I'm using the TAS5782MEVM Board for development. Unfortunately the EEPROM on the board has been damaged (unable to read/write anymore, even with an external EEPROM reader). I've replaced the EEPROM with the same type.
Since then, I'm unable to work with PPC3, since during "Tuning and Audio Processing" it gets stuck at "Writing coefficents to device". In the System Check, it tells me that the FWID is invalid (most likely due to the empty EEPROM).
Is there any chance to get the binary of the original EEPROM for reflashing? Or is there at least a way to write the FWID, if yes, to which memory location?
Seems a bit unreasonable for me to dump a $200 Eval Board due to a $1 EEPROM...
Kind regards,
Stefan Oechslein