Other Parts Discussed in Thread: TAS5342, TAS5548
Hi Experts:
Customer want use TAS5558 + TAS5342 for 5.1 speakers.
Customer have bought TAS5548EVM, it can work normally with the control of the GUI. But, after use TAS5558 for the replacement, then GUI display a message that USB is connected but no device found on 0x34. We make sure the ASEL pin is low.
Switch back to the original TAS5548 chip, the TAS5548EVM also can work normally.
Is there any difference between TAS5558 and TAS5548? Is there something else need to modify?