This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am using the PCM1795 and I am supplying clocks and data but don't get an analog output. All analog outputs are at a current of -1.2mA no matter the digital input. Some more parameters of my setup:
* 32bit, right-justified format
* SYCLK = 5MHz
* BCK = 1.25MHz
* LRCK = 19.53125kHz (Note: _not_ an audio application so non-standard sample rate.
* All clocks verified using logic analyzer
* All registers in their default state except register 18 where I set FMT to 001
** I can read back the register contents periodically and the values are correct.
** If I send 0x9200 to the control port I get back 0x0010.
* Reset conditions have been checked. Delay between reset and configurationis long enough. Configuration is kept so assumed OK.
* All power supplies within +-1% of nominal
How can I proceed debugging this issue? Is there any way to read out the status of the baudrate auto-detect?
Best regards,
Matthias
Hello,
I continued debugging the analog circuit with another OP amp today. I am using the circuit described here:
https://e2e.ti.com/support/data_converters/audio_converters/f/64/t/235364
The TIA op amp has rail-to-rail inputs and outputs. I tried different values for the biasing the TIA's + pin but I never get the correct 0 scale current. Could you provide an equivalent circuit of the DAC's current outputs clearly indicating the direction of the specified output current please? I want to be 100% sure that I understand the output.
Best Regards,
Matthias
Hi Matthias,
The current will ways be flowing out of the device. The voltage potential on the left side of Rf should be higher than the right side. Can you note on the schematic the values you are using for Rf, the divider resistors, and the resistors in the differential stage?
Thanks!