This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: Selection of Audio Codec: Speaker + External Amplifier

Other Parts Discussed in Thread: PCM5101A, TLV320DAC3203, PCM5121, TLV320DAC3120, TPA2013D1

Tool/software: Linux

Hi,

We planned to integrate a Analog Speaker(DAC) Device. Below are our requirements,

1. Codec Chipset(No Internal Apmlifier) + External Amplifier.

2. Type : Stereo.

3. No of Digital Input : 2

4. No of Analog Output : 2

5. No of DAC : 2

6. Control Interface : I2C

7. Sampling Frequency : Should support from Min - 8KHz to Max - 96KHz

8. SNR: 106 dB, Typical

9. Bit Resoluction : 16, 24.

10. Should support Volume Control

Could anyone able to help us to reach the product(Audio Codec + External Amplifier) depending upon our above requirements