HI All,
I have two quesionts,
1. Can TAS5782M supports 3-WIRES I2S with 96K sample rate, we found 30wires works well with 48K sample rate,but there is not output with 96K
2. How can TAS5782M hardware connected with TDM, is it the same as I2S hardware connection and only need to set the R40 configuration ?
3. If the input TDM is 4 channel ,since TAS5782 only support 2.0, is it possible for TAS5782M support this type TDM and how to let it work?
Thanks!