This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5751M-TAS5733L-SW: 3-wire I2S support?

Part Number: TAS5751M-TAS5733L-SW
Other Parts Discussed in Thread: TAS5733, PCM2706, TAS5713, TAS5751M, TAS5733L

On page 1 of the datasheets of both TAS5733 and TAS5751, it is claimed that the devices support 3-wire I2S (no MCLK needed), however there does not seem to be another word on that in the datasheets.

Is this a similar story as the related post on the TAS5713: 3-wire I2S only with a SCLK = MCLK rate of >2.1MHz, so Fs=44.1/48kHz 16 bit is not feasible, so input from an USB codec like PCM2706 is not feasible?