This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5766M: Need TAS5766M Efficiency with 4ohm Load, 17V PVCC Conditions

Part Number: TAS5766M

Hi Sirs,

Would you pls manage TAS5766M efficiency with 4ohm load, 17V PVCC condition? Before the actual number, can I assume the TAS5766M's efficiency around 70% (between 12V and 24V's curve) with 2W, 4ohm load?



Thank you and Best regards,

Wayne Chen
06/20/2018