This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
we have a question regarding the overcurrent function (cycle by cycle) and the resistor Roc: Is it correct that this function changes depending on BTL and PBTL?
According to datasheet, if using 2 x BTL and max output is 300W/pr.channel into 4 ohm, max current should then be totally 17A. When Roc is 22k, then according to datasheet current limit is15A. This should indicate that for BTL, 22k will limit max current to 15A pr.channel?
According to datasheet, if using 1 x PBTL and max output is 400W into 3ohm, max current should then be totally 11,5A. Then the 22k setting limits current to 15A for this single channel.
The max. value for the overcurrent resistor Roc is given to be 33k in the datasheet. Some time ago we got a diagram from TI that showed overcurrent limit vs. Roc. According to this diagram, if 40k is selected the limit for a DKD package will be 11,5A. Is 40k allowed? What is the approximate tolerance in percent ?
regards
Trond Inge Wang
Trond,
The OC limit is always per each output. I'm not sure of the diagram that was shared with you, can you tell me where this came from?
Regards,
-Adam
Hi Adam,
I got this diagram from someone at TI and stored it on my PC, but I was unable to find the mail.
The diagram is inserted and is a .pdf file. If the file insertion did not function, I can send it by mail, but I need your address.
regards
Trond Inge Wang8737.TAS5630-1-Nom-OC-Trip-110401.pdf