Hello
My customer is using TAS5508C and in the market.
It may be special case, but customer has pop issue from the market
in case very low level sound with low volume .
So far, customer had been set 0x14 as 14h [ D4=1].
When customer tested 0x14h as 04h [D4=0], pop with automute improved.
Do you agree?”
In TAS5508C data sheet , ”Set input automute threshold less than bit 1 (zero input signal), lowest automute threshold."
in booth of the D4=1, D=0 case.
Best Regards