Hello, i have a problem with TAS5721 generating quite loud thump sound in the speakers when exiting shutdown mode. Board is designed according to "2.1 system" application note from the data sheet. System is in 2.1 mode, so i have removed SSTIMER cap according to the data sheet, and i'm enabling mid-Z ramp feature when exiting shutdown, by writing 0x84 to register 0x05. Still i get quite loud thump during shutdown exit (during shutdown enter after playing some sound on amp, there is only barely audible click, so the problem is only related to shutdown exit). Is there anything i could do to minimize this unwanted thump?
Thanks,
WM