Other Parts Discussed in Thread: INA163
Hi team,
My customer has a requirement for a low noise audio amp. The amp is used to convert the differential signal from MIC to single ended signal. The gain is set to 1V/V and the input signal is -41dBv, 100Hz~10kHz.
Customer required that the amp total noise is under -106dBV. And the SNR needs to be higher than 65dB when the input is -41dBV. The power supply of the amp is single supply @3~3.3V. Do you think the TL972 is suitable? If not, do you have any other recommendation? Thanks.
Best regards,
Wayne