Other Parts Discussed in Thread: TPA6133A2, TPA6138A2, TPA6141A2
Hi TI Support,
Question to Idd supply current to the TPA6132A. I'm very confusing to the data sheet and EVM documents.
From The TPA6132A2 Data sheet, I read that, Table 2, Design Parameter Shown Current is only 3mA to 3.2mA, with input voltage range from 2.2V to 5.3V.
But, on the TPA6132A2 EVM document specified the supply current Idd =0.5A Maximum.
Please confirm that why the values were a lot different.
I do want to have a low current supply for driving 2 X32 Ohm speakers of the headset, please provide me which is the best solution?
Thanks