This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRC4382EVM-PDK: installing the USB-MODEVM driver

Part Number: SRC4382EVM-PDK

Hi

I am struggling to install the USB drivers for the SRC4382EVM-PDK.

I have followed the instructions in the User guide (section 3.3), but the device is recognized as a Human interface device, not a NI-VISA USB device as the guide says is required.

the USB-MODEVM_WDM.inf file is in the C:/Windows/inf directory, and is installed, but when I try to update the driver, USB-MODEVM does not appear as an option.

Where am i going wrong?

I have tried on both windows xp and windows 10 32bit, the result is the same on both.

Thanks

Ben