This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am tasked with designing a Universal Front End preamplifier audio product and we have the PCM1863 and DIR9001PWR IC.
We have a prototype setup but need the Software to Control and Configure the PCM1863: Software-Controlled Audio ADC for production.
Please provide the software so we can Control and Configure the PCM1863, thank you.
Best Regards,
Neil Henry
IRAD LLC
"Systems Design House"
Hi Neil,
click on the "request" button on this page. once you've requested access, the request goes to export control for approval, this can take a day or two.
Once approved the software will appear on your myTI account under My SecureSoftware.
best regards,
-Steve Wilson
Hi Steve,
We did this last year for another project with the PCM5142 IC and was shutdown, request denied! So we went with AKM device. This was embarrassing for us as a Texas design shop!
Now we will give it another shot, thank you. I will make the request again.
Neil
IRAD
Getting this error. Please see attached file. Thanks.
Hmm....not allowing attachment of error on making the SW request.
Neil,
I've just sent you a PM with my email address. Please send the error to me and lets figure out what is keeping you from receiving approval.
We want your business. Let's figure out what is going on and why you didn't receive approval for the software. I hate to hear that something like this would keep you from using our product.
FYI, There is a new family of ADCs being released that meet or exceed the performance of the PCM186x family, the power consumption is considerably lower, package size smaller, and the price should be very competitive.
Here is a link to the TLV320ADC3140 preview. This is the first device that will release, you will see some higher performance previews from the same family of devices in the coming weeks.
best regards,
-Steve Wilson
Hi Steve,
We are configuring the PCM1863 to exercise the "Integrated High-Performance Audio PLL" feature? What is the default ADC sample resolution - 192KHZ?
Also what HW Control use to exercise the SW-Controlled Gain?
How can we setup for I2S streaming this IC without SW Control?
We are using the DIR9001 as the front end for 96KHZ and the AK4113 DIR for 192KHZ.
FLOW:
AK4113 > PCM1863 > PCM5102
Presently we are trying to test device as default.
Regards
Neil
What is the default wiring to the PCM5102A?
Systems Interaction Diagram:-
PC/CELL PHONE SOURCE > PCM1863 > PCM5102A
Wired as datasheet Figure 66, however PIN 14 high 3.3V.
Thanks
Neil
Neil,
Can you clarify your question? your question seems really simple.
PCM1863 || PCM5102
DOUT || DIN
BCLK || BCLK
LRCLK || LRCLK
best regards,
-STeve Wilson
Hello Steve,
I am looking for a wiring validation of the circuit wiring and configuration.
Presently we have:
CIRCUIT: PCM1863 >I2S> PCM5102A
The PCM1863 DEFAULT circuit is wired as in datasheet as Slave PLL MODE. However not working!
Please see datasheet Figure 66. The only difference is PIN 14 wired HIGH 3.3V.
What is the setup for PCM5102A i.e. hook-up/wiring?
We need to validate this setup and test as the DEFAULT. Note no I2C configuration has been done. Just need to baseline the PCM1863 DEFAULT circuit as is from TI OEM.
Thank you.
Neil
Hi Neil,
So you have the PCM5102A set up as the I2S master? what are the MCLK, BCLK and WCLK frequencies from the PCM5102A?
best regards,
-Steve Wilson
Neil,
You also said that the PCM1863 was in slave mode, which means it isn't providing any clocks. So where are the clocks coming form?
I need clear and precise information or I can't help you.
best regards,
-Steve Wilson
Neil,
Were you able to find any more information about this?
best regards,
-Steve Wilson
We have decided to look for a hardware controlled audio ADC. Thank you.
Client have changed their requirements.
Neil